This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

sema4_uboot

Overview

The sema4 uboot example shows how to use SEMA4 driver to lock and unlock a sema gate, the notification IRQ is also demonstrated in this example. This example should work together with uboot. This example runs on Cortex-M core, the uboot runs on the Cortex-A core.

Supported Boards