This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

snvs_hp_hac

Overview

The SNVS HP HAC project shows how to use the High Assurance Counter (HAC) based on SDK SNVS HP driver. In this example,

  1. The HAC is enabled and set a initial value.

  2. Software fatal security violation is triggered, and the SSM switches to soft fail mode.

  3. In soft fail mode, software stops the HAC counter, and clear the HAC to make SSM switch to hard fail mode.

  4. The system resets when enters hard fail mode.

Supported Boards