This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

spi_interrupt

Overview

The spi_interrupt example shows how to use spi functional API to do interrupt transfer:

In this example, one spi instance as master and another spi instance as slave. Master sends a piece of data to slave, and check if the data slave received is correct.

Supported Boards