This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tmu_2_monitor_threshold

Overview

The TMU example shows how to configure TMU register to monitor and report the temperature from multiple temperature measurement sites strategically located on the chip.

The TMU has access to multiple temperature measurement sites strategically located on the chip. It monitors these sites and can signal an alarm if a programmed threshold is ever exceeded.

Supported Boards