This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

trdc

Overview

The Multicore TRDC demo application demonstrates how to use TRDC on a multicore system to control the access policy of the memory block checker(MBC) and memory region checker(MRC), and how to configure the domain access control(DAC) for bus masters to access both secure and non-secure domains.

First, the primary core example uses 1 domain for secure access demo. The primary core which is secure first sets a MRC memory region and a MBC memory block to non-secure access only, then trys to access the memory which triggers the hardfault. In hardfault the access control is changed to secure access to resolve the error. Then, the primary core releases the secondary core from the reset. The secondary core example uses 2 domains, one is for secure access and the other is for non-secure access. By enabling different DAC configuration, different domain is used for the access control. The secure access process is the same as the primary core. In the non-secure access demo, the secondary core sets a MRC memory region and a MBC memory block to secure access only, and switch to the non-secure DAC configuration which force the core to be non-secure. Then trys to access the memory which triggers the hardfault. In hardfault certain flags stored in flash is set to let primary core know and update the configuration to non-secure access to resolve the error, because the TRDC is secure access only.

Supported Boards