This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tsc_debugMode

Overview

The fourWireModeInterrupt example shows how to use TSC driver in 4-wire debug modes: The touch screen controller needs to co-work with ADC and TSC analogue.

In this example , we make use of the available electrodes on board to show driver usage.

  1. Firstly, before TSC starts work, ADC driver configure ADC_HCx;

  2. Then, we configure TSC module to work in debug mode.

  3. Then, we configure six states(1st-pre-charge, 1st-detect, x-measure, y-measure, and 2nd-pre-charge, 2nd-detect) to simulate non-debug(hardware) mode.

  4. Lastly, if measure data is valid, serial terminal prints x/y-coordinate information.

Running the demo

When running successfully, the log output in terminal shall be similar as below:

TSC DebugMode Example Start! ADC_5HC_DoAutoCalibration() Done. Please touch screen! x = 234, y = 3655 x = 239, y = 3715 x = 236, y = 3708 x = 236, y = 3667 x = 236, y = 3653 x = 236, y = 3628 x = 233, y = 3637 x = 236, y = 3680 …

Supported Boards