This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tsens_interrupt

Overview

The tsens_interrupt example shows how to configure TSENS register to measure the temperature through a high-precision zoom-ADC.

In this example, it shows how to init and configure the TSENS model and get the temperature value from the register when the application is ready.