This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tsi_v4_low_power_mode

Overview

The tsi_v4_low_power example shows how to use TSI_V4 driver in low power modes:

In this example , we make use of the available electrodes on board to show driver usage.

  1. Firstly, we get the non-touch calibration results as baseline electrode counter;

  2. Then, we start the Hardware-Trigger scan using interrupt method to wakeup from low power modes through pad touch;

  3. Note: you can select which low power mode you want to enter into.

Running the demo

When running successfully, the log output in terminal shall be similar as below:

TSI_V4 Low_Power_Modes Example Start! Please don’t touch the touchpad. Press anykey to start TSI low power example. Start calibartion…. Calibrated counters for channel 0 is: 2772 Calibrated counters for channel 1 is: 65535 Calibrated counters for channel 2 is: 65535 Calibrated counters for channel 3 is: 65535 Calibrated counters for channel 4 is: 65535 Calibrated counters for channel 5 is: 65535 Calibrated counters for channel 6 is: 2965 Calibrated counters for channel 7 is: 2642 Calibrated counters for channel 8 is: 2682 Calibrated counters for channel 9 is: 2901 Calibrated counters for channel 10 is: 65535 Calibrated counters for channel 11 is: 2708 Calibrated counters for channel 12 is: 2958 Calibrated counters for channel 13 is: 5072 Calibrated counters for channel 14 is: 421 Calibrated counters for channel 15 is: 5073

Let’s move to the low power modes world!!!

Press specific key to enter stop mode. After enter stop modes, touch PAD XX to wakeup.

Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into STOP MODE! Great!!! You touched it!!!

Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into VLPS MODE! Great!!! You touched it!!!

Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into LLS MODE! Wakeup will lead to a interrupt flow, pay attention to it!!! Great!!! You touched it!!!

Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into VLLS1 MODE! Wakeup will lead to a reset flow, pay attention to it!!!

Wake up from VLLSx modes…

TSI_V4 Low_Power_Modes Example Start! Please don’t touch the touchpad. Press anykey to start TSI low power example. …… ……

Supported Boards