This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

xspi_psram_polling_transfer

Overview

The xspi_psram_polling_transfer example shows how to use xspi driver with polling:

In this example, xspi will send data and operate the external PSRAM connected with XSPI. Some simple flash command will be executed, such as Read Data and Write Data. Example will write/read through the whole chip, through IP command and AHB command.

Supported Boards