This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

aoi_input_mux

Overview

The INPUT_MUX AOI demo application demonstrates the use of CMP and SCTIMER AOI peripherals. The example Use the output of cmp and sctimer as the input of the aoi function. When the input voltage of cmp changes, The output of cmp changes, which changes the output of aoi.
The purpose of this demonstration is to show how to use the AOI driver in the SDK software.

Run the demo

The VREF voltage is half of the reference voltage.

After the demonstration runs successfully, you can see the following information on the oscilloscope:

CMP input voltage is less than the VREF voltage, AOI has no waveform output
CMP input voltage is greater than the VREF voltage, AOI continuous output square wave

Supported Boards