This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

aoi_io_and

Overview

The AOI IO_AND demo application demonstrates the use of IO and AOI peripherals. The example Use the two IO as the input of the aoi function: AOI_OUT = (IO0 & IO1). When IO0 and IO1 are both high level, the AOI_OUT is high level. When any of IO is low level, the AOI_OUT is low level. The purpose of this demonstration is to show how to use the AOI driver in the SDK software.

Run the demo

After the demonstration runs successfully, you can see the following information in the terminal window:

aoi_io_and project.

Supported Boards