This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

csi_ccir656

Overview

The CSI CCIR656 project shows how to receive the camera data using CSI driver, the camera interface is CCIR656. In this example, you will see the camera input image shown in the LCD. Please note that the camera input image resolution might be smaller than the LCD panel, so part of the LCD panel might be blank.

Supported Boards