This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

csi_fragment_gray

Overview

The csi_fragment_gray project shows how to use CSI driver fragment mode functions. In this example, the camera input format is YUV422, the CSI driver extracts the Y element of a specific window (gray image). To show gray image, ELCDIF LUT is used. If this example runs successfully, you will see a gray image window in the middle of the LCD panel. The image is updated each time input any value from debug console.

Please note that only one frame buffer is used in this example, so there might be screen tearing.

Supported Boards