This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

qtmr_inputcapture

Overview

The QTMR project is a demonstration program of the SDK QTMR driver’s input capture feature by DMA. The example sets up a QTMR channel for input capture. Once the input signal is received, this example will print the capture value.

Supported Boards