This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

qtmr_outputpwm

Overview

The QTMR project is a demonstration program of the SDK QTMR driver’s output variable frequency pwm feature by interrupt. The example also up one QTMR channel to output pwm. The user should probe a 50Khz PWM signal output with 50% dutycycle with a oscilloscope. The user can enter a value to update the Duty cycle.

Supported Boards