This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dspi_dma_b2b_transfer_slave

Overview

The dspi_dma_b2b_transfer example shows how to use DSPI driver in dma way:

In this example , we need two boards, one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_dma_b2b_transfer_slave.c’ includes the DSPI slave code.

  1. DSPI on master board send/received data to/from DSPI on slave board in dma.

  2. DSPI on slave board using dma to receive/send the data