This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexcan_pretended_networking_wakeup

Overview

The flexcan_pretended_networking_wakeup example shows how to wake up FLEXCAN module from Pretended Networking mode:

In this example, 2 boards are connected through CAN bus. Endpoint B need enter STOP mode first, then endpoint A(board A) send CAN Message to Endpoint B(board B) when user press space key in terminal. Endpoint B will wake up from STOP mode after receive 4 specific wake up frame, and print the message content to terminal.

Supported Boards