This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

usart_sync_transfer_slave

Overview

The uart synchronous transfer slave example shows how to use usart driver in synchronous way:

In this example, one USART is configured as master node and another is configured as slave node. Master will send data to slave firstly, and then receive data from slave, slave board will send back the received data.

Supported Boards