This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexio_spi_edma_lpspi_transfer_slave_dynamic

Overview

The flexio_spi_edma_lpspi_transfer_slave_dynamic example shows how to use flexio spi slave driver in edma way:

In this example, a flexio simulated slave connect to a lpspi master. The CS signal remains low during transfer, after master finishes the transfer and re-asserts the CS signal, interrupt is triggered to let user know.

Supported Boards