This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

i2c_accel_event_trigger

Overview

This example demonstrate how to wake up main device in low power mode with accelerometer trigger event. The accelerometer can keep working while the main device is in low power mode (or deep sleep mode). Only when the configured event was captured, the accelerometer will trigger the interrupt to wake up the main device. This example uses I2C to configure the accelerometer to work in 800Hz data rate with low noise mode. And when the tap event is triggered, it will wake up the main device. And 32 samples around the trigger event will be captured.

Supported Boards