This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

i2c_read_fxls897x_accel_value_transfer

Overview

The i2c_read_fxls897x_accel_value example shows how to use I2C driver to communicate with an i2c device:

  1. How to use the i2c driver to read a i2c device who_am_I register.

  2. How to use the i2c driver to write/read the device registers.

In this example, the values of three-axis accelerometer print to the serial terminal on PC through the virtual serial port on board.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C example – Read Accelerometer Value Found an FXLS8974 on board, the device address is 0x18. The accel values: x = -31 , y = -39 , z = 1301 x = -31 , y = -39 , z = 1301 x = -20 , y = -23 , z = 1305 x = -20 , y = -23 , z = 1305 x = -20 , y = -23 , z = 1305 x = -24 , y = -12 , z = 1275 x = -24 , y = -12 , z = 1275 x = -28 , y = -27 , z = 1290 x = -28 , y = -27 , z = 1290 x = -16 , y = -20 , z = 1316

End of I2C example.

Supported Boards