This is the documentation for the latest (main) development branch of
     mcuxpresso sdk. If you are looking for the documentation of previous releases, use
     the drop-down menu on the left and select the desired version.
    
  
  
           
             
  
cmp
Overview
The cmp input external example demonstrates the comparator’s functionality with two external voltage source, the example detect high level interrupt and lower level interrupt.