This is the documentation for the latest (main) development branch of
mcuxpresso sdk. If you are looking for the documentation of previous releases, use
the drop-down menu on the left and select the desired version.
The cmp input internal example demonstrates the comparator’s functionality with one external voltage source and one internal voltage reference source, the example detect rising edge interrupt and falling edge interrupt.