This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpc_i2c_dma_b2b_slave

Overview

The i2c_dma_b2b_transfer_slave example shows how to use i2c driver as slave to do board to board transfer with a DMA master:

In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. I2C slave works as supporting board to help demonstrate master DMA trasnfer, actually uses interrupt way.

Supported Boards