This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

usart_transfer_dma

Overview

This example shows how to use the DMA driver to implement a double buffer receive scheme from the USART The example shows the double buffer constructed using two descriptors (g_pingpong_desc). These descriptors are cycled from one to the other.

Things to note :

  • The descriptors of the ping pong transfer need to be aligned to size 16

  • The initial transfer will perform the same job as first descriptor of ping pong, so the first linkeage is to go to g_pingpong_desc[1]

  • g_pingpong_desc[1] then chains the g_pingpong_desc[0] as the next descriptor

  • The properties are set up such that g_pingpong_desc[0] (and the initial configuration uses INTA to signal back to the callback)

  • g_pingpong_desc[1] uses INTB to signal to the callback

  • The scheduled callback uses this information to know which data was last written

A note on Performance : The intent of this example is to illustrate how a double-buffer scheme can be implemented using the dma. The performance of this example will be limited to how quickly the echo printer can read-out the data from the ping pong buffer and display it. This means that the example will work well if characters are entered at a rate where the DMA callback to echo the string can keep up with the input stream. Connecting the USART RX to a continuous fast speed will cause the DMA to fall behind.

Supported Boards