This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

usart_transfer_rb_dma

Overview

The usart dma ring buffer example shows how to use usart driver with DMA driver used:

In this example, a ring buffer was implemented to receive the characters from PC side, to implemente the ring buffer, a descriptor was created and chain itself as the next descriptor, then the DMA transfer will start a continuous transfer.

While data in the ring buffer reach 8 characters, routine will send them out using DMA mode.

Supported Boards