This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpit_pwm

Overview

This demo show how to use SDK drivers to implement the PWM feature by LPIT IP module in dual 16-bit Periodic counter mode,and clone by TRGMUX to output this PWM to TRGMUX_OUTx pin. By default,the pwm duty is 50%, user can input from terminal to change the period and duty cycle,use oscilloscope can measure this output PWM signal.

Supported Boards