This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpit_single_channel

Overview

The LPIT single channel project is a simple example of the SDK LPIT driver. It sets up the LPIT hardware block to trigger a periodic interrupt after every 1 second. When the LPIT interrupt is triggered a message a printed on the serial terminal and an LED is toggled on the board.

Running the demo

When the example runs successfully, you can see an LED is toggled on the board and see the similar information from the terminal as below.

Starting channel No.0 … Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred ! Channel No.0 interrupt is occurred !

Supported Boards