This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpspi_3wire_edma_transfer_slave

Overview

The lpspi_3wire_edma_transfer example shows how to use LPSPI’s 3-wire mode in edma way:

In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘lpspi_3wire_edma_transfer_slave.c’ includes the LPSPI slave code.

  1. LPSPI master send/received data to/from LPSPI slave in edma . (LPSPI Slave using edma to receive/send the data)

  2. LPSPI master will use SOUT pin as input/output pin, and slave will use SIN pin as input/output pin.

Supported Boards