This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpuart_9bit_transfer

Overview

The lpuart_9bit_transfer example shows how to use lpuart driver in 9-bit mode.

In this example, one lpuart instance is used with 9bit mode. Its TX and RX pins are connected together. The data with 9bit can be received by itself. The each data in TX and RX data register will be 16-bit data.

Supported Boards