This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpuart_polling_seven_bits

Overview

The lpuart_polling_seven_bits Example project is to demonstrate usage of the KSDK lpuart driver with seven data bits feature enabled. In the example, you can send characters to the console back and they will be printed out onto console instantly. NOTE: Please set com port format to “7 data bits without parity bit” in PC’s com port tool

Supported Boards