This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ltc_aes

Overview

This project is a demonstration program that uses the KSDK software for encryption/decryption sample data using AES-CBC, AES-CCM, and XCBC-MAC algorithm.

Running the demo

When the demo runs successfully, from the terminal you can see:

……………………….. LTC (AES) DRIVER EXAMPLE ………………………..

Testing input string: Once upon a midnight dreary, while I pondered weak and weary, Over many a quaint and curious volume of forgotten lore, While I nodded, nearly napping, suddenly there came a tapping, As of some one gently rapping, rapping at my chamber door Its some visitor, I muttered, tapping at my chamber door Only this, and nothing more.

———————————– AES-CBC method ————————————– AES CBC Encryption of 320 bytes. AES CBC encryption finished.

AES CBC Decryption of 320 bytes. AES CBC decryption finished. Decrypted string : Once upon a midnight dreary, while I pondered weak and weary, Over many a quaint and curious volume of forgotten lore, While I nodded, nearly napping, suddenly there came a tapping, As of some one gently rapping, rapping at my chamber door Its some visitor, I muttered, tapping at my chamber door Only this, and nothing more.

———————————– AES-CCM method ————————————– AES CCM Encryption of 320 bytes. using iv length : 12 bytes using aad length : 20 bytes using key length : 16 bytes using tag length : 8 bytes AES CCM encryption finished.

AES CCM decryption of 320 bytes. AES CCM decryption finished. Decrypted string: Once upon a midnight dreary, while I pondered weak and weary, Over many a quaint and curious volume of forgotten lore, While I nodded, nearly napping, suddenly there came a tapping, As of some one gently rapping, rapping at my chamber door Its some visitor, I muttered, tapping at my chamber door Only this, and nothing more.

———————————– AES-CMAC —————————————— AES CMAC Computing hash of 320 bytes Computed hash: ba fd 2c 65 a 62 7c 18 a0 df b4 20 bb fb 68 27

………….. THE END OF THE LTC (AES) DRIVER EXAMPLE …………………………..

Supported Boards