This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ltc_aes_edma

Overview

This project is a demonstration program that uses the KSDK software for encryption/decryption sample data using EDMA for AES-CBC algorithm.

Running the demo

When the demo runs successfully, from the terminal you can see:

……………. LTC (AES EDMA) DRIVER EXAMPLE ………………………..

Testing input string: Once upon a midnight dreary, while I pondered weak and weary, Over many a quaint and curious volume of forgotten lore, While I nodded, nearly napping, suddenly there came a tapping, As of some one gently rapping, rapping at my chamber doorIts some visitor, I muttered, tapping at my chamber doorOnly this, and nothing more.

————————- AES-CBC method ————————————– AES CBC Encryption of 320 bytes. AES CBC encryption finished.

AES CBC Decryption of 320 bytes. AES CBC decryption finished. Decrypted string : Once upon a midnight dreary, while I pondered weak and weary, Over many a quaint and curious volume of forgotten lore, While I nodded, nearly napping, suddenly there came a tapping, As of some one gently rapping, rapping at my chamber doorIts some visitor, I muttered, tapping at my chamber doorOnly this, and nothing more.

………….. THE END OF THE LTC (AES EDMA) DRIVER EXAMPLE ………….

Supported Boards