This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mcg_pee_blpi

Overview

The pee_bpli example shows how to use MCG driver to change from PEE mode to BLPI mode:

  1. How to use the mode functions for MCG mode switch.

  2. How to use the frequency functions to get current MCG frequency.

  3. Work flow Boot to PEE mode from default reset mode Change mode PEE -> PBE ->FBE -> FBI -> BLPI Change back BLPI -> FBI -> FBE -> PBE -> PEE Get System clock in PEE mode to blink LED

In this example, because the debug console’s clock frequency may change, so the example running information is not output from debug console. Here the LED blinks to show that the example finished successfully.

Supported Boards