This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

spi_interrupt_b2b_master

Overview

The spi_interrupt_b2b_master example shows how to use spi functional API to do interrupt transfer as a master:

In this example, the spi instance as master. Master sends a piece of data to slave, receive data from slave,and check if the data master received is correct. This example needs to work with spi_interrupt_b2b_slave example.

Supported Boards