This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dpu_1_warp

Overview

This project shows the arbitrary warping function of fetch warp unit.

The DPU path is configured like this:



  • Coordinate buffer * * Frame buffer *



      |                                          |
      v                                          v

+—————–+ +—————–+ | | | | | Fetch Eco9 |———————->| FetchRot9 | | | | | +—————–+ +—————–+ | +—————–+ | | | Store9 | | | +—————–+ | *********************** * * * output buffer * * * *********************** | | +—————–+ +—————–+ | | | | | FetchYUV0 | | Const Frame 0 | | | | | +—————–+ +—————–+ | | | v | +—————–+ | | | +———>| LayerBlend 1 | | | +—————–+ | v +—————–+ | | | ExtDst0 | | | +—————–+ | Content v +—————–+ | | | FrameGen 0 | | | +—————–+ | v

Supported Boards