This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ftm_input_capture

Overview

The FTM project is a demonstration program of the SDK FTM driver’s input capture feature. The example sets up a FTM channel for dual-edge capture. Once the input signal is received, this example will print the capture value.

Supported Boards