This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ftm_simple_pwm

Overview

The FTM project is a simple demonstration program of the SDK FTM driver. It sets up the FTM hardware block to output a center-aligned PWM signal. The PWM dutycycle is periodically updated. On boards that have an LED connected to the FTM pins, the user will see a change in LED brightness.

Note

If the FTM instance has only TPM features, please use the TPM driver. Can be judged by FSL_FEATURE_FTM_IS_TPM_ONLY_INSTANCE(base) macro.

Supported Boards