This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ftm_timer

Overview

The FTM project is a simple demonstration program of the SDK FTM driver to use FTM as a timer. It sets up the FTM hardware block to trigger an interrupt every 1 millisecond. When the FTM interrupt is triggered 1000 times, a message is printed on the UART terminal.

Supported Boards