This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

jpegdec_context_switch

Overview

The SD JPEG decoder example decodes a series of JPEG pictures stored on SD card then shows them one by one on panel. Two slots are used and each has one descriptor linked to itself. After slot 0 finishes slot 1 will be switch on in this round. After slot 1 finishes then the next round starts, slot 0 will be switched on again.

Supported Boards