This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

jpegdec_single_stream_repeat

Overview

The SD JPEG decoder example decodes a series of JPEG pictures stored on SD card then shows them one by one on panel. Only one slot is used with two descriptors linked with each other as ping-pong descriptors. After one descriptor finishes the other will be loaded.

Supported Boards