This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

qsci_dma_transfer

Overview

The qsci_dma_transfer example shows how to use QSCI driver in DMA way: In this example, one qsci instance is connected to PC,the board will send back all characters that PC sends to the board. Note : The example echo every 8 characters, so input 8 characters every time.

Supported Boards