This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

qsci_interrupt_transfer

Overview

The qsci_interrupt example shows how to use qsci driver in interrupt way:

In this example, one uart instance is connected to PC, the board will send back all characters that PC sends to the board.

Note: The example echoes every 8 characters, so input 8 characters every time.

Supported Boards