This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

qsci_edma_rb_transfer

Overview

The qsci_edma_rb_transfer example demonstrates the usage of the KSDK QSCI EDMA driver. In this example, a ring buffer is used with EDMA enabled, data received will be stored in ring buffer first, while IDLE line is detected, the received characters will be read out, and echo them back to the terminal using EDMA method.

Supported Boards