This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

jpegdec_single_stream_single_frame_descriptor

Overview

The JPEG decoder example decodes one JPEG picture using slot 0 then shows it on panel. First we configure the descriptor, then enable the descriptor to let it update the decoder configuration and start decode. After decoding complete the picture will be shown on panel.

Supported Boards