This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tpm_output_compare

Overview

The TPM project is a demonstration program of the SDK TPM driver’s output compare feature. It sets up one TPM channel to toggle the output when a match occurs with the channel value. The user should probe the TPM output with a oscilloscope to see the signal toggling.

Supported Boards