This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tpm_timer

Overview

The TPM project is a simple demonstration program of the SDK TPM driver to use TPM as a timer. It sets up the TPM hardware block to trigger an interrupt every 1 millisecond. When the TPM interrupt is triggered 1000 times, a message is printed on the UART terminal.

Supported Boards