This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tpm_simple_pwm

Overview

The TPM project is a simple demonstration program of the SDK TPM driver. It sets up the TPM hardware block to output a center-aligned PWM signal(24kHZ). The PWM duty cycle is manually updated and is initially 10%. On boards that have an LED connected to the TPM pins, the user will see a change in LED brightness if user enter different values.

Supported Boards