This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tpm_pwm_twochannel

Overview

The TPM project is a simple demonstration program of the SDK TPM driver. It sets up the TPM hardware block to output PWM signals(24KHZ) on two TPM channels. The PWM dutycycle on both channels is manually updated. The example sets up a TPM channel-pair to output two edge-aligned PWM signals. On boards that have an LED connected to the TPM pins, the user will see a change in LED brightness if user enter different values.

Supported Boards