This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tpm_combine_pwm

Overview

The TPM project is a demonstration program of generating a combined PWM signal by the SDK TPM driver. It sets up the TPM hardware block to output PWM signals(24kHZ) on two TPM channels. The example also show’s the complementary mode of operation and deadtime insertion. The PWM duty cycle is manually updated and is initially 10%. On boards that have 2 LEDs connected to the TPM pins, the user will see a change in LED brightness if user enter different values. And if the board do not support LEDs to show, the outputs can be observed by oscilloscope.

Supported Boards